2.3 Remote Controller Connection

Note

The remote controller is pre-paired at the factory and does not require re-pairing. Simply press the central PS5-logo button to quickly establish a connection.


2.3.1 Operation Steps

1. Open the “Add Robot” page

Enter the Bluetooth connection interface

Enter the Bluetooth connection interface

2. After connecting to the robot, go to Robot Settings → Bluetooth → Select the controller to connect

Tap Bluetooth settings

Tap Bluetooth settings

3. Select the controller and tap to connect

Select the controller and tap to connect

Select the controller and tap to connect