2.4 Shutdown Guide

2.4.1 Assist the Robot to Lie Down (No Gantry Required)

Important

After the robot switches into the Standing Preparation (Position-Control Standing) mode and before it is fully laid on the ground, ensure one or two operators assist in keeping the robot stable and balanced.


Step 1: Enter Standing Preparation Mode (Position-Control Standing)

  • Short-press [L2 + X] on the controller to switch the robot into Standing Preparation (Position-Control Standing) mode.

  • During the operation, manually support the robot from the rear handle to prevent imbalance or falling.

Step 2: Lay the Robot Down

  • Slowly lower the robot from the standing posture in Standing Preparation mode to the ground, ensuring a controlled and steady movement.

  • Have at least two operators assist to avoid the robot tipping or entering an abnormal posture during the process.

Step 3: Enter Zero-Torque Mode

  • After ensuring the robot is stable and facing forward, switch it to Zero-Torque Mode using the remote controller to ensure safe shutdown.

  • During the state transition, support the robot from the rear handle or secure its back against a chair to maintain balance.


Recommended Procedure (Safer):

  • First switch to Damping Mode: short-press [L2 + R2 + Create] on the controller.

  • Then switch to Zero-Torque Mode: short-press [L1 + R1 + Create] on the controller.

Emergency Stop Procedure: If an immediate stop is required, directly switch to Zero-Torque Mode via the controller.

Step1:shutdown1

Step 4: Power Off

  • Short-press the power button on the back of the battery to wake the device, then long-press for about 5 seconds to shut it down.

  • During shutdown, the LED1–4 indicators on the battery will turn off sequentially, indicating the device has powered off.

Step 4: Press the Power Button

Step 4: Press the Power Button

Step 5: Pack the Robot as Illustrated

  • Open the side door of the packaging case and ensure sufficient space for placing the robot inside.

  • Follow the illustrated steps: place the robot’s legs into the positioning slot first, then fold and place the upper body into the case.

  • Ensure all parts of the robot are securely positioned in the slots, then close and lock the case.

Step 5: Packing

2.4.2 Shutdown from Sitting Posture (No Gantry Required)

Step 1: Use the Controller to Make the Robot Sit

  • Short-press [L2 + ←] on the controller to trigger the robot’s sitting action.

  • Place the robot on a stable platform or stool with a height of 35–40 cm to ensure proper support.

Step 1: Trigger the Sitting Motion via Controller

Step 1: Trigger the Sitting Motion via Controller

Step 2: Enter Zero-Torque Mode

  • Ensure the robot is sitting stably and facing forward, then switch to Zero-Torque Mode with the controller for safe shutdown.

  • During the state transition, support the robot from the rear handle or ensure its back rests securely against a chair to prevent falls in Zero-Torque Mode.


Recommended Procedure (Safer):

  • Switch to Damping Mode first: short-press [L2 + R2 + Create].

  • Then switch to Zero-Torque Mode: short-press [L1 + R1 + Create].

Emergency Stop: If immediate stopping is required, directly switch to Zero-Torque Mode via the controller.


Step 3: Power Off

  • Short-press the power button on the back of the battery to wake the device, then long-press for about 5 seconds to shut it down.

  • During shutdown, the LED1–4 indicators on the battery will turn off sequentially, indicating the device has powered off.

Step 3: Press the Power Button

Step 3: Press the Power Button

Step 4: Pack the Robot as Shown

  • Open the side door of the packaging case and ensure sufficient space for placing the robot inside.

  • Follow the illustrated steps: place the robot’s legs into the positioning slot first, then fold and place the upper body into the case.

  • Ensure all parts of the robot are securely positioned in the slots, then close and lock the case.

shutdown_3

Important

  • During the sitting operation, ensure the robot is securely positioned on a 35–40 cm-high stool or platform with proper back support.

  • When switching from sitting posture to Zero-Torque Mode, manually support the robot from the rear handle to maintain balance and prevent falls.