4.7 Code Implementation
Note
This section applies only to X2 Ultra and X2 Ultra(new version). X2 EDU has no interaction computing unit and supports neither speech playback nor facial expression control, so this section does not apply.
In this section, you will develop a simple robot control program that makes robot X2 perform a sequence of hand motions and speech playback.
4.7.1 Project Overview
In this project, we will develop a Python program that uses ROS 2 interfaces to control robot X2 to perform the following action sequence:
Execute the first action (wave)
Speech playback
Execute the second action (handshake)
Prerequisite: As in the previous section, the robot must be in the Stable Standing Mode.
This project will help you understand how to use the SDK to control the robot’s hand motion sequence and interaction features, laying the groundwork for more complex tasks.
4.7.2 Add the Example to the Existing SDK Workspace
We will add a new example program to the existing SDK workspace, which allows you to:
Reuse the existing build system
Keep code organization consistent
Simplify the build and run workflow
Understand the Existing Structure
The SDK workspace has the following structure:
aimdk/
├── src/
│ ├── examples/ # C++ examples
│ │ ├── src/
│ │ │ ├── hal/ # Hardware Abstraction Layer examples
│ │ │ ├── mc/ # Motion control examples
│ │ │ └── interaction/ # Interaction feature examples
│ │ └── CMakeLists.txt
│ └── py_examples/ # Python examples
│ ├── py_examples/
│ └── setup.py
Caution
Notes about non-volatile user data:
The disks in the robot would be reformatted during firmware upgrade/downgrade, please back up your data
User data under
$HOME(/home/agi, compatible path /agibot/data/home/agi) would survive in generalException 1: DO NOT save data into
$HOME/aimdk*, which are preserved and maintained by the systemException 2: All data under
$HOMEwould be moved to$HOME/.old_agi_home.bak(specific to v1.0 firmware flashing)BE CAREFUL of features like factory reset, which would forcibly erase all user data (including
$HOME)
Add a New Python Example
We will add a new example program under the py_examples directory:
# Go to the SDK directory
# Replace the path below with your actual extracted path
cd /path/to/aimdk
# Create a new example file under py_examples
touch src/py_examples/py_examples/action_sequence_demo.py
4.7.3 Write the Control Code
Caution
As standard ROS DO NOT handle cross-host service (request-response) well, please refer to SDK examples to use open interfaces in a robust way (with protection mechanisms e.g. exception safety and retransmission)
While the robot is in Stable Standing Mode or Locomotion Mode, DO NOT launch ROS nodes in rapid bulk (no more than 2 nodes per second is recommended), as a large number of nodes joining DDS discovery within a short period causes communication congestion and degrades motion control real-time performance, which may cause the robot to lose balance and fall
Create the Robot Control Class
In src/py_examples/py_examples/action_sequence_demo.py, add the following code:
#!/usr/bin/env python3
import rclpy
from rclpy.node import Node
import time
from aimdk_msgs.srv import SetMcPresetMotion, PlayTts
from aimdk_msgs.msg import (
RequestHeader, McPresetMotion, McControlArea, CommonState,
TtsPriorityLevel
)
class ActionSequenceDemo(Node):
def __init__(self):
super().__init__('action_sequence_demo')
# Create service clients
self.set_preset_motion_client = self.create_client(
SetMcPresetMotion, '/aimdk_5Fmsgs/srv/SetMcPresetMotion')
self.play_tts_client = self.create_client(
PlayTts, '/aimdk_5Fmsgs/srv/PlayTts')
self.get_logger().info('Action Sequence Demo created')
# Wait for services to become available
while not self.set_preset_motion_client.wait_for_service(timeout_sec=1.0):
self.get_logger().info('Waiting for preset motion service...')
while not self.play_tts_client.wait_for_service(timeout_sec=1.0):
self.get_logger().info('Waiting for TTS service...')
def perform_preset_motion(self, area_id, motion_id):
"""Execute a preset motion"""
request = SetMcPresetMotion.Request()
request.header = RequestHeader()
request.header.stamp = self.get_clock().now().to_msg()
motion = McPresetMotion()
motion.value = motion_id
area = McControlArea()
area.value = area_id
request.motion = motion
request.area = area
request.interrupt = False
self.get_logger().info(f'Executing preset motion: area={area_id}, motion={motion_id}')
future = self.set_preset_motion_client.call_async(request)
rclpy.spin_until_future_complete(self, future)
if future.result() is not None:
response = future.result()
if response.response.header.code == 0:
self.get_logger().info('Preset motion executed successfully')
return True
else:
self.get_logger().error('Preset motion execution failed')
return False
else:
self.get_logger().error('Failed to call preset motion service')
return False
def speak(self, text):
"""Trigger TTS speech output"""
if not self.play_tts_client.wait_for_service(timeout_sec=5.0):
self.get_logger().error('TTS service unavailable')
return False
request = PlayTts.Request()
request.header.header.stamp = self.get_clock().now().to_msg()
# Configure TTS request
request.tts_req.text = text
request.tts_req.domain = 'action_sequence_demo' # Caller identifier
request.tts_req.trace_id = 'sequence' # Request ID
request.tts_req.is_interrupted = True # Allow interrupting same-priority speech
request.tts_req.priority_weight = 0
request.tts_req.priority_level = TtsPriorityLevel()
request.tts_req.priority_level.value = 6 # Priority level
self.get_logger().info(f'TTS speak: {text}')
future = self.play_tts_client.call_async(request)
rclpy.spin_until_future_complete(self, future, timeout_sec=10.0)
if future.result() is not None:
response = future.result()
if response.tts_resp.is_success:
self.get_logger().info('Speech playback succeeded')
return True
else:
self.get_logger().error('Speech playback failed')
return False
else:
self.get_logger().error('Failed to call TTS service')
return False
def wave_hand(self):
"""Control robot to wave hand"""
# Use preset motion: right-hand wave (area=2, motion=1002)
return self.perform_preset_motion(2, 1002)
def shake_hand(self):
"""Control robot to perform handshake"""
# Use preset motion: right-hand handshake (area=2, motion=1003)
return self.perform_preset_motion(2, 1003)
def perform_action_sequence(self):
"""Execute the complete action sequence"""
self.get_logger().info('Starting action sequence...')
self.get_logger().info('Prerequisite: robot must be standing')
# 1. First action: Wave hand
if not self.wave_hand():
self.get_logger().error('Wave hand failed')
return False
time.sleep(5)
# 2. TTS speech
if not self.speak('Hello! I am AgiBot X2. Now demonstrating a hand action sequence!'):
self.get_logger().error('TTS failed')
return False
time.sleep(3)
# 3. Second action: Handshake
if not self.shake_hand():
self.get_logger().error('Handshake failed')
return False
time.sleep(3)
self.get_logger().info('Action sequence completed')
return True
Add the Main Entry Point
In the same file, add the main entry point:
def main(args=None):
rclpy.init(args=args)
demo = ActionSequenceDemo()
# Execute the action sequence
demo.perform_action_sequence()
# Shut down the ROS node
demo.destroy_node()
rclpy.shutdown()
if __name__ == '__main__':
main()
Register in the Build System
To run the new example with the ros2 run command, you need to add an entry point in setup.py:
# In src/py_examples/setup.py, add this to entry_points:
"action_sequence_demo = py_examples.action_sequence_demo:main",
The complete entry_points section should include:
entry_points={
"console_scripts": [
# ... existing entries ...
"action_sequence_demo = py_examples.action_sequence_demo:main",
],
},
4.7.4 Build and Run
Build the Project
# Go to the SDK directory
# Replace the path below with your actual extracted path
cd /path/to/aimdk
# Set environment variables
source /opt/ros/humble/setup.bash
# Build the project
colcon build --packages-select py_examples
Run the Project
# Set environment variables
source install/local_setup.bash
# Run the new example program
ros2 run py_examples action_sequence_demo
4.7.5 Code Walkthrough
Robot Control Class
The ActionSequenceDemo class is the core of the robot’s control system and provides the following capabilities:
Initialize ROS node and service clients: The constructor creates the ROS node and the required service clients.
Execute preset motions: The
perform_preset_motionmethod is used to execute predefined motions.Voice broadcast: achieve TTS audio output through the
speakmethodControl robot actions: Methods such as
wave_handandshake_handare provided to control the robot’s hand motions.Execute the action sequence: The
perform_action_sequencemethod runs the sequence wave → speak → handshake in order.
4.7.6 Extensions and Optimization
Add More Actions and Interactions
You can extend the existing code to add more robot actions and interaction features, for example:
Blow a kiss (preset motion ID: 1004)
Salute (preset motion ID: 1013)
Heart gesture (preset motion ID: 1007)
Raise hand (preset motion ID: 1001)
Additional speech content
Expression control
And so on
Add Parameter Configuration
You can use the ROS 2 parameter system to make action parameters configurable:
# Declare parameters in the constructor
self.declare_parameter('wave_count', 3)
self.declare_parameter('wait_duration', 3.0)
# Use parameters in your methods
wait_duration = self.get_parameter('wait_duration').value
time.sleep(wait_duration)
Add Error Handling
You can refer to the example Get Robot Mode to add more error-handling logic and make the program more robust:
def send_request(self):
request = GetMcAction.Request()
request.request = CommonRequest()
self.get_logger().info('📨 Sending request to get robot mode')
for i in range(8):
request.request.header.stamp = self.get_clock().now().to_msg()
future = self.client.call_async(request)
rclpy.spin_until_future_complete(self, future, timeout_sec=0.25)
if future.done():
break
# retry as remote peer is NOT handled well by ROS
self.get_logger().info(f'trying ... [{i}]')
response = future.result()
if response is None:
self.get_logger().error('❌ Service call failed or timed out.')
return
self.get_logger().info('✅ Robot mode get successfully.')
self.get_logger().info(f'Mode name: {response.info.action_desc}')
self.get_logger().info(f'Mode status: {response.info.status.value}')
Add More Interaction Features
You can integrate additional interaction features:
# Add an expression service client
from aimdk_msgs.srv import PlayEmoji
# Add expressions in the action sequence
def show_expression(self, emoji_id):
# Implement expression control here
pass
# Add multiple speech messages
def speak_multiple_messages(self, messages):
for message in messages:
self.speak(message)
time.sleep(1)
4.7.7 Troubleshooting
First, check the FAQ section. If the issue is still not resolved, consider contacting AgiBot X2 technical support.
4.7.8 Next Steps
After completing this section, you can:
Explore more examples: Review other example programs under
src/py_examples/py_examples/orsrc/examples/src/.Integrate perception features: Learn how to access and process sensor data.
Develop more complex tasks: Combine multiple functional modules to build more complex robot applications.
4.7.9 Summary
By now, you have learned how to:
✅ Add a new example program to an existing SDK workspace
✅ Execute a preset motion sequence
✅ Implement TTS speech playback
✅ Build and run a custom example program
✅ Control a sequence of hand motions for the robot: wave → speak → handshake
Congratulations! You have now mastered the basic development skills for the AgiBot X2 AimDK, including motion control, speech interaction, and action-sequence orchestration, and you are ready to start building your own robot applications!