4.1 Read the user guide to familiarize yourself with relevant terminology and safety precautions.


4.2 Complete the basic system configuration

  • Operating System: Ubuntu 22.04 LTS

  • ROS 2 Version: Humble

  • Python Version: Python 3.8 or later

  • C++ Standard: C++17

And SDK example dependencies:

  • OpenCV: Image processing

  • Ruckig: Trajectory generation

  • ncurses: Terminal control

  • libcurl: Network communication

  • cv_bridge: ROS–OpenCV image conversion

Depending on how you use the SDK, the scenarios are as follows:

  • SDK-on-device mode: the development computing unit already includes all prerequisites, so no installation is required. (Recommended for quick start.)

  • PC-side SDK + cross-device networking mode: ensure the host PC meets the above requirements.

Host PC installation reference

4.3 Network connection

The AgiBot X2 Ultra supports multiple network access methods to connect to the onboard system:

(1) Direct wired connection via the rear Ethernet port — Connect a network cable between the robot’s SDK development Ethernet port and the host PC.

  • Configure the host PC network interface to a static IP (10.0.1.2, subnet mask 255.255.255.0).

  • The development computing unit will then be accessible at 10.0.1.41, enabling cross-device ROS networking and SSH login (credentials require technical support).

(2) Wi-Fi connection through the robot’s built-in hotspot

  • Enable the AP Hotspot in the robot APP, and check the Wi-Fi SSID and password.

  • After connecting to the hotspot, you can access the development computing unit via the jump host at 192.168.88.88 (SSH credentials require technical support).


Attention

Taking Motion Control Computing Unit(PC1, 10.0.1.40) as build & run environment for secondary development is strictly prohibited to avoid safety risks

Attention

For PC-side SDK + cross-device networking, use a wired direct connection. Wi-Fi should only be used for SSH debugging.

Important

It is not recommended to place the robot and development PC on a public or complex network with other devices. Developers must properly manage network security risks to prevent communication interference or data leakage.

4.4 Environment installation and configuration

Place the SDK into the target environment and extract it.

# Set environment variables (this step can be skipped when running directly on the development computing unit)
source /opt/ros/humble/setup.bash

# Build the SDK
# Assume the extracted top-level directory for the X2 AimDK project is named 'aimdk'
cd ./aimdk/
colcon build

Caution

Notes about non-volatile user data:

  • The disks in the robot would be reformated during firmware upgrade/downgrade, please backup you data

  • User data under $HOME(/agibot/data/home/agi) would suervive in general

  • Exception 1: DO NOT save data into $HOME/aimdk*, which are preserved and maintained by the system

  • BE CAREFUL of features like factory reset, which would force erase all user data (include $HOME)