5.4.1 Sensor Interfaces

The sensor interfaces provide data access and control for the robot’s various sensors, including cameras, IMUs, LiDAR, and touch sensors.

Core Features

Vision Sensors

  • RGB Camera: Captures color images

  • Depth Camera: Provides depth information

  • Camera Intrinsics: Retrieves calibration parameters

Pose Sensors

  • IMU Data: Acceleration, angular velocity, and attitude angles

  • Gyroscope: Measures angular velocity

  • Accelerometer: Measures acceleration

Environmental Perception Sensors

  • LiDAR: Provides point cloud data

  • Touch Sensors: Tactile feedback

Standard Sensor Messages

Most sensor interfaces use the standard message types defined in ROS sensor_msgs:

Sensor Data Type

Message Definition

Camera intrinsics

CameraInfo

Raw image

Image

Compressed image

CompressedImage

IMU data

Imu

LiDAR point cloud

PointCloud2

IMU Topics

Includes chest IMU and torso IMU, both located on the development compute unit (PC2).
You can also use the IMUs integrated in LiDAR and the RGB-D camera.

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/imu/chest/state

Imu

Chest IMU data

TRANSIENT_LOCAL

500Hz

/aima/hal/imu/torso/state

Imu

Torso IMU data

TRANSIENT_LOCAL

500Hz

/aima/hal/sensor/lidar_chest_front/imu

Imu

LiDAR IMU data

TRANSIENT_LOCAL

200Hz

/aima/hal/sensor/rgbd_head_front/imu

Imu

RGB-D camera IMU data

RELIABLE

200Hz

Head Touch Status Topic

Supported features:

  • Access low-level touch events and raw samples

  • Disable the built-in “head pat” skill (to be enabled)

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/sensor/touch_head

TouchState

Head touch status

TRANSIENT_LOCAL

100Hz

  • TouchState ros2-msg @ hal/msg/TouchState.msg

    # Head touch status
    # Topic: /aima/hal/sensor/touch_head
    
    MessageHeader header             # Message header
    uint8 event_type                 # Touch event (0-unknown, 1-idle, 2-touch, 3-slide, 4-single tap, 5-double tap, 6-triple tap)
    uint32[8] data                   # Raw sensor values for 8 channels
    uint32[8] threshold              # Touch thresholds for 8 channels
    bool[8] is_touched               # Touch state of 8 channels
    

Rear RGB Camera Topics

The rear RGB camera is on the development compute unit (PC2) and can be used for visual localization assistance and semantic scene understanding.
Raw image bandwidth is about 90 MB/s — use only on the same compute unit, do not subscribe across units.

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/sensor/rgb_head_rear/camera_info

CameraInfo

Camera intrinsics

RELIABLE+TRANSIENT_LOCAL

N/A

/aima/hal/sensor/rgb_head_rear/rgb_image

Image

Raw image

TRANSIENT_LOCAL

10Hz

/aima/hal/sensor/rgb_head_rear/rgb_image/compressed

CompressedImage

Compressed image

TRANSIENT_LOCAL

10Hz

Note: The handle behind AgiBot X2’s neck would obstruct the view of Rear RGB Camera partially. If your vision algorithms affected by this, please refer to Rear Head Monocular Camera Data Subscription to mask obstructed area of images

Obstructed view of Rear RGB Camera on default head posture:

后视RGB相机遮挡示意图

Rear RGB Camera - Obstructed View Diagram

Stereo Camera Topics

The stereo camera is on the development compute unit (PC2) and can be used for stereo vision, teleoperation, obstacle perception, object recognition, VIO SLAM, VLA and more.
Raw image bandwidth is about 90 MB/s per eye — use only on the same compute unit, do not subscribe across units.

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/sensor/stereo_head_front_left/camera_info

CameraInfo

Left camera intrinsics

RELIABLE+TRANSIENT_LOCAL

N/A

/aima/hal/sensor/stereo_head_front_left/rgb_image

Image

Left raw image

TRANSIENT_LOCAL

10Hz

/aima/hal/sensor/stereo_head_front_left/rgb_image/compressed

CompressedImage

Left compressed image

TRANSIENT_LOCAL

10Hz

/aima/hal/sensor/stereo_head_front_right/camera_info

CameraInfo

Right camera intrinsics

RELIABLE+TRANSIENT_LOCAL

N/A

/aima/hal/sensor/stereo_head_front_right/rgb_image

Image

Right raw image

TRANSIENT_LOCAL

10Hz

/aima/hal/sensor/stereo_head_front_right/rgb_image/compressed

CompressedImage

Right compressed image

TRANSIENT_LOCAL

10Hz

RGB-D Camera Topics

The RGB-D camera is on the development compute unit (PC2) and can be used for object detection, spatial obstacle avoidance, and semantic environment understanding.
Raw image bandwidth is about 25 MB/s per stream — use only on the same compute unit, do not subscribe across units.

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/sensor/rgbd_head_front/rgb_camera_info

CameraInfo

RGB intrinsics

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/rgb_image

Image

Raw image

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/rgb_image/compressed

CompressedImage

Compressed image

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/depth_camera_info

CameraInfo

Depth intrinsics

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/depth_image

Image

Depth image

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/depth_pointcloud

PointCloud2

Depth point cloud

RELIABLE

10Hz

/aima/hal/sensor/rgbd_head_front/imu

Imu

IMU data

RELIABLE

200Hz

LiDAR Topics

Provides LiDAR point clouds and LiDAR-integrated IMU data for obstacle avoidance and SLAM/localization.
The LiDAR is on the development compute unit (PC2) with data bandwidth on the order of 10 MB/s — cross-unit subscriptions are not recommended.

Topic Name

Data Type

Description

QoS

Frequency

/aima/hal/sensor/lidar_chest_front/lidar_pointcloud

PointCloud2

LiDAR point cloud

TRANSIENT_LOCAL

10Hz

/aima/hal/sensor/lidar_chest_front/imu

Imu

LiDAR IMU data

TRANSIENT_LOCAL

200Hz

Code Examples

For detailed code samples and explanations, see:

Safety Notes

Attention

  • For high-bandwidth raw camera streams, do not subscribe across compute units; this may destabilize the system and create safety risks.