5.1.6 Joint Control
The joint control interfaces provide precise control over each robot joint, supporting multiple control modes and joint groups.
Key Features
Control Modes
Position Control: Drive a joint to a specified target angle.
Velocity Control: Drive a joint at a specified angular velocity.
Torque Control: Command a joint to output a specified torque.
Supported Joints
Left Arm Joints: 7-DoF (3 shoulder joints, 1 elbow joint, 3 wrist joints).
Right Arm Joints: 7-DoF (3 shoulder joints, 1 elbow joint, 3 wrist joints).
Left Leg Joints: 6-DoF (3 hip joints, 1 knee joint, 2 ankle joints).
Right Leg Joints: 6-DoF (3 hip joints, 1 knee joint, 2 ankle joints).
Waist Joints: Yaw, pitch, and roll.
Head Joints: PitchN.Y.A., and yaw
Joint Control Topics
Joints are controlled by body part (arms, legs, waist, head), and closed-loop control can be implemented using status feedback.
Topic Name |
Data Type |
Description |
QoS |
Frequency |
|---|---|---|---|---|
|
|
Joint control commands |
- |
Hz |
|
|
Joint state feedback |
|
Hz |
Here, * can be head (requires supported head hardware), arm, waist, or leg.
JointCommandArrayros2-msg @ hal/msg/JointCommandArray.msg# Joint control command array MessageHeader header # Message header JointCommand[] joints # Joint command array
JointCommandros2-msg @ hal/msg/JointCommand.msg# Joint control command string name # Joint name (optional) float64 position # Position (rad) float64 velocity # Velocity (rad/s) float64 effort # Torque (N·m) float64 stiffness # Stiffness (N·m/rad) float64 damping # Damping (N·m·s/rad)
The length and ordering of
JointCommand[]are defined in the table below.Joint group
Length
Contents
Notes
head
2
head_yaw,head_pitchonly yaw now, and pitch is unavailable
waist
3
wrist_yaw,wrist_pitch,wrist_rollarm
7*2
shoulder_pitch,shoulder_roll,shoulder_yaw,elbow,wrist_yaw,wrist_pitch,wrist_rollAll left-side joints first, then all right-side joints
leg
6*2
hip_pitch,hip_roll,hip_yaw,knee,ankle_pitch,ankle_rollAll left-side joints first, then all right-side joints
JointStateArrayros2-msg @ hal/msg/JointStateArray.msg# Joint state array MessageHeader header # Message header DomainErrorState state # Joint error state JointState[] joints # Joint state array
DomainErrorStateros2-msg @ hal/msg/DomainErrorState.msg# Joint error state uint8 value # 1: Damping, 2: PowerOff, 3: Disabled, 4: Communication Failed, Others: NA
JointStateros2-msg @ hal/msg/JointState.msg# Joint state information string name # Joint name (currently unused) float64 position # Position (rad) float64 velocity # Velocity (rad/s) float64 effort # Torque (N·m) uint8 coil_temp # Coil temperature (°C) uint8 motor_temp # Motor temperature (°C) uint8 motor_vol # Motor voltage (V)
The length and ordering of
JointState[]follow theJointCommand[]joint ordering described in Joint Order.
Joint State Query Service
Service Name |
Data Type |
Description |
|---|---|---|
|
|
Actively query joint states |
GetAllJointStateros2-srv @ hal/srv/GetAllJointState.srv# Get all joint states # Service: /aimdk_5Fmsgs/srv/GetAllJointState # Request CommonRequest request # Common request # Response CommonResponse reponse # Common response JointState[] head_joints # Head joint states JointState[] arm_joints # Arm joint states JointState[] waist_joints # Waist joint states JointState[] leg_joints # Leg joint states
The length and ordering of
JointState[]follow theJointCommand[]joint ordering description above.
Programming Examples
For detailed examples and code explanations, refer to:
C++ Example: Robot Joint Control Example
Python Example: Robot joint control example
Safety Notes
Warning
Joint Limits
All joints have motion range limits; exceeding them may cause mechanical damage.
It is recommended to check that joint angles are within their safe ranges before sending commands.
Be especially cautious about safety limits when using torque control.
Caution
As standard ROS DO NOT handle cross-host service (request-response) well, please refer to SDK examples to use open interfaces in a robust way (with protection mechanisms e.g. exception safety and retransmission)
Note
Best Practices
Use smooth trajectory planning to avoid sudden joint motions.
Implement joint state monitoring and anomaly detection.
Ensure the robot is in a safe state before issuing control commands.