5.2.2 Screen Control

The screen control interface provides full display control capabilities, including emoji playback, video playback, and more. It enables developers to implement rich visual interaction features for the robot.

Key Features

  • Playback of multiple preset emoji expressions

  • Custom video playback

  • Playlists (coming soon) and loop playback

  • Playback priority control

Emoji Playback Status Topic

Topic Name

Data Type

Description

QoS

Frequency

/face_ui_proxy/status

FaceEmojiStatus

Emoji playback status

RELIABLE

1Hz

  • FaceEmojiStatus ros2-msg @ face_ui/FaceEmojiStatus.msg

    # Emoji Status Info
    
    MessageHeader header             # Message header
    string e_path                    # Path of the emoji file
    string[] e_path_list             # List of emoji paths in the current sequence
    uint8 e_id                       # Emoji ID
    uint8 mode                       # Playback mode (1: once, 2: loop)
    int32 priority                   # Priority
    uint8 status                     # Current status (0: idle, 1: start, 2: running, 3: completed, 4: stopped)
    float64 time_to_end_ms           # Remaining time (seconds)
    

    status special notes:

    • The following states are edge-triggered (reported only once):

      • 1 - start, 3 - completed, 4 - stopped

Emoji Playback Service

Service Name

Data Type

Description

/aimdk_5Fmsgs/srv/PlayEmoji

PlayEmoji

Play emoji

  • PlayEmoji ros2-srv @ face_ui/srv/PlayEmoji.srv

    # Play Emoji
    # Service: /aimdk_5Fmsgs/srv/PlayEmoji
    
    # Request
    CommonRequest header  # Request header
    
    uint8 emotion_id  # Emoji ID
    uint8 mode  # Playback mode (1: once, 2: loop)
    int32 priority  # Playback priority
    
    ---
    
    # Response
    CommonResponse header  # Response header
    
    bool success  # Whether the command succeeded
    string message
    

    emotion_id Emoji Mapping Table:

    Emoji ID

    Emoji name

    Description

    1

    Blink

    Basic blink action

    10

    Calm - eye variation 1

    Eye variation for calm state

    11

    Calm - eye variation 2

    Eye variation for calm state

    20

    Calm - game

    Game-state emoji

    30-33

    Calm - cute

    Cute expression series

    40

    Close eyes

    Close-eye action

    50

    Open eyes

    Open-eye action

    60

    Bored

    Bored expression

    70

    Abnormal

    Abnormal state

    80

    Sleeping

    Sleeping state

    90

    Happy

    Happy expression

    100-101

    Extra happy / ecstatic

    Extremely happy expression

    110

    Sad

    Sad expression

    120

    Sympathy

    Sympathetic expression

    130

    Confused

    Confused expression

    140

    Shocked

    Shocked expression

    150

    Acting cute

    Cute/affectionate expression

    160

    Serious

    Serious expression

    170

    Thinking

    Thinking expression

    180

    Angry

    Angry expression

    190

    Extra angry

    Extremely angry expression

    200

    Adoration

    Adoring expression

    210

    Extra adoring

    Extremely adoring expression

    220

    Charging

    Charging state

    priority Priority Mechanism Explanation:

    • This priority mechanism applies to emoji playback (PlayEmoji) and video playback (PlayVideo).

    • If the new request’s priority is not lower than the current one, it overrides the current request.

    • If the new request’s priority is lower, it is ignored.

Video Playback Service

Service Name

Data Type

Description

/aimdk_5Fmsgs/srv/PlayVideo

PlayVideo

Play video

/aimdk_5Fmsgs/srv/PlayVideoGroup

PlayVideoGroup

Play a list of videos

  • PlayVideo ros2-srv @ face_ui/srv/PlayVideo.srv

    # Play Video
    # Service: /aimdk_5Fmsgs/srv/PlayVideo
    
    # Request
    CommonRequest header             # Request header
    string video_path                # Absolute path of video file (must be on the interaction compute unit and readable by all)
    uint8 mode                       # Playback mode (1: once, 2: loop)
    int32 priority                   # Playback priority
    
    # Response
    CommonResponse header            # Response header
    bool success                     # Whether playback succeeded
    string message                   # Response message
    

    Notes:

    • By default, video playback does not include audio.

    • Audio and video files must use absolute paths.

    • Audio and video files must be stored on the interaction compute unit (PC3, 10.0.1.42), not the development compute unit (PC2).

    • Audio and video files (and all parent directories up to root) must be readable by all users(new subdirectory under /var/tmp/ is recommended)

  • PlayVideoGroup ros2-srv @ face_ui/srv/PlayVideoGroup.srv

    # Play Video
    # Service: /aimdk_5Fmsgs/srv/PlayVideoGroup
    
    # Request
    CommonRequest header             # Request header
    string[] video_path_list         # List of absolute path of video files (must be on the interaction compute unit and readable by all)
    uint8 mode                       # Playback mode (1: once, 2: loop)
    int32 priority                   # Playback priority
    
    # Response
    CommonResponse header            # Response header
    bool success                     # Whether playback succeeded
    string message                   # Response message
    

    Notes:

    • see notes of PlayVideo >>

Programming Examples

For detailed code examples and explanations, refer to:

Safety Notes

Warning

Display Control Limitations

  • Emoji playback occupies display resources; manage resources carefully.

  • Video playback requires correct and accessible file paths.

  • Set priorities properly to avoid conflicts.

Caution

As standard ROS DO NOT handle cross-host service (request-response) well, please refer to SDK examples to use open interfaces in a robust way (with protection mechanisms e.g. exception safety and retransmission)

Note

Best Practices

  • Use appropriate playback modes to avoid unnecessary looping.

  • Monitor display states and handle exceptions.

  • Implement content queueing for better control.

  • Ensure correct file paths and formats.