5.1.3 MC Control Signal Configuration

MC control signal configuration provides unified management of multiple input sources, ensuring the robot always responds to the highest-priority control signal.

Control signal configuration is one of the core features of the AgiBot X2 AimDK, enabling unified management and priority arbitration among multiple control sources. This mechanism ensures that when multiple control inputs are active, the robot safely and reliably responds to the command with the highest priority.

Key Features

Multi-Source Integration

  • RC Control: PS5 remote controller (priority 80)

  • VR Control: Teleoperation control (priority 70)

  • App Control: Control via the mobile app (priority 60)

  • Voice Control: Voice-command control (priority 50)

  • …

  • SDK Customization: Developer-defined control sources (priority 20–100, configurable)

Priority Management

  • Dynamic Adjustment: Priority can be modified at runtime.

  • Automatic Arbitration: Automatically selects the highest-priority active input source.

  • Conflict Resolution: If multiple sources share the same priority, the earliest active source is selected.

Input Source Configuration

Priority Reference

  • 100–80: System-level control (emergency stop, safety modes)

  • 79–60: High-level control (remote controller, mobile app)

  • 59–40: Mid-level control (voice, gestures)

  • 39–20: Low-level control (SDK custom development sources)

  • 19–0: Backup control (debugging, testing)

Arbitration Workflow

Arbitration Mechanism

Input Source Arbitration and Management Rules:

  • Commands from disabled or unknown input sources are discarded.

  • Among valid sources, the system selects the one with the highest priority and accepts only its commands.

  • If a new active source with a higher priority appears, it immediately replaces the current one.

  • If the selected input source becomes inactive (timeout, etc.), it is treated as lowest priority and re-selection occurs.

Note: After a system restart, all input-source priority states reset.

Modules developed via SDK should register a unique input source name and assign an appropriate priority (recommended 20–100).

The built-in control input sources are listed below:

source

Description

Priority

Timeout (ms)

rc

Remote controller

80

1000

app_proxy

Agibot Go mobile app

60

1000

vr

Teleoperation module

70

1000

interaction

AgiBot Interaction module

50

1000

pnc

AgiBot Planner module

40

1000

Input Source Management Services

Service Name

Data Type

Description

/aimdk_5Fmsgs/srv/GetCurrentInputSource

GetCurrentInputSource

Query the current control input source

/aimdk_5Fmsgs/srv/SetMcInputSource

SetMcInputSource

Configure input source

  • GetCurrentInputSource ros2-srv @ mc/motion/srv/GetCurrentInputSource.srv

    # Get current control input source
    # Service: /aimdk_5Fmsgs/srv/GetCurrentInputSource
    
    # Request
    CommonRequest request        # Standard request header
    
    ---
    
    # Response
    CommonTaskResponse response  # response.header.code = 0 indicates success
    McInputSource input_source   # Current input source
    
    • McInputSource ros2-msg @ mc/motion/McInputSource.msg

      string name               # Name of the currently selected input source (e.g., rc/vr/app_proxy/...)
      int32 priority             # Configured priority (0–100)
      int32 timeout              # Configured timeout (ms)
      
  • SetMcInputSource ros2-srv @ mc/motion/srv/SetMcInputSource.srv

    # Service: /aimdk_5Fmsgs/srv/SetMcInputSource
    
    # Request
    CommonRequest request        # Standard request header
    McInputAction action         # Operation type (ADD/MODIFY/DELETE/DISABLE/ENABLE)
    McInputSource input_source   # Input source
    
    ---
    
    # Response
    CommonTaskResponse response  # response.header.code = 0 indicates success
    
    • McInputAction ros2-msg @ mc/motion/McInputAction.msg

      int32 value  # Operation type (1001: ADD, 1002: MODIFY, 1003: DELETE, 2001: ENABLE, 2002: DISABLE)
      

    Operation Type (Value)

    Description

    Required field(s) in input_source

    ADD (1001)

    Add new input source

    name, priority, timeout

    MODIFY (1002)

    Modify existing input source

    name, priority, timeout

    DELETE (1003)

    Delete input source

    name

    ENABLE (2001)

    Enable input source

    name

    DISABLE (2002)

    Disable input source

    name

Programming Examples

For detailed programming examples and code explanations, refer to:

Notes

Important

Version Compatibility: MC control signal configuration is available only in X2_AimDK v0.7 and later; it is not supported in v0.6 or earlier.

Attention

SDK modules should register a unique input-source name based on the system modules list and assign an appropriate priority (recommended 20–100).

Caution

As standard ROS DO NOT handle cross-host service (request-response) well, please refer to SDK examples to use open interfaces in a robust way (with protection mechanisms e.g. exception safety and retransmission)

Note

Before the motion-control system receives any valid input (e.g., after power-on with no movement and all commanded velocities being zero), querying the current input source may return empty.